Time Synchronization view
- On the explorer bar, select
Devices. - InDevices, double-click the controller to open the device profile.
- In the device profile, selectTime Synchronization.
Use the
Time Synchronization
view to view time synchronization status
and enable or disable time synchronization on the controller. Enabling time synchronization
allows the controller to participate as a clock in the system time. It also allows the
controller to become a master clock for the system, or become a master clock in the
chassis.If the controller is the grandmaster clock, all devices connected to the controller
synchronize with the clock of the controller. The
Time Synchronization
view displays details for the device that is acting as the grandmaster clock.Provide Feedback