Windowxx view parameters

The
Windowxx
view includes these parameters:
Parameter
Description
Window Mode
Displays the mode that the window is configured for.
Output On Value
Displays the value that defines one side of the window thresholds.
The outputs (if tied to the window) and I.Windowxx.InWindow tag switch state at this threshold according to the diagram Figure 1.
Output Off Value
Output On Hysteresis
Displays the negative offset from the Output On Value to apply hysteresis to.
Output Off Hysteresis
Displays the negative offset from the Output Off Value to apply hysteresis to.
Outputs Controlled by this Window
Output00
Determines whether this window controls the indicated output.
Outputs Controlled by this Window
Output01
Determines whether this window controls the indicated output.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal