Windows view parameters

The
Windows
view includes these parameters:
Parameter
Description
Window
Displays the window number to which this configuration applies.
Mode
Displays which input tag value the window operates on.
Unit
Displays the unit that is associated with the configured Mode for the window.
Output On Value
Displays the value that defines one side of the window thresholds.
The outputs (if tied to the window) and I.Windowxx.InWindow tag switch state at this threshold according to the diagram Figure 1.
Output Off Value
Output On Hysteresis
Displays the negative offset from the Output On Value to apply hysteresis to.
Output Off Hysteresis
Displays the negative offset from the Output Off Value to apply hysteresis to.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal