Events view parameters

The
Events
view include these parameters:
Parameter
Description
Member Name
Value
Event
The event number to which this configuration applies.
Enable Event
Displays whether the corresponding event trigger is active. Events are triggered when conditions match the event definition.
EO.Eventxx.En
  • 0 = Event trigger definition is not active and events are not triggered when conditions match the definition
  • 1 = Event trigger definition is active and events are triggered when conditions match the definition
Latch Event
Displays whether an event is latched until it is acknowledged.
EO.Eventxx.LatchEvent
  • 0 = Event is not latched. New events overwrite old events.
  • 1 = Event is latched. Events are latched until acknowledged. New events are not reported until the current event is acknowledged. Up to four new events are stored in the memory buffer. When the memory buffer is full, additional events are lost.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal