Counter Diagnostics dialog parameters

The
Counter Diagnostics
dialog includes these parameters:
Parameter
Description
Fault Exists
Displays whether a fault is present.
Data Uncertain
Displays whether the counter is operating outside the designed operating range, or data is under manual or override control.
Field Power
Displays whether field power is present on the counter.
Field Power On Timestamp
Displays the timestamp of the last time field power turned on in YYYY-MM-DD-HH:mm:SS.mmm format.
  • YYYY = year
  • MM = month
  • DD = day
  • HH = hour (24 hour)
  • mm = minutes
  • SS = seconds
  • mmm = milliseconds
You can see a valid time or None if no event time is recorded.
Field Power Off Timestamp
Displays the timestamp of the last time field power turned off in YYYY-MM-DD-HH:mm:SS.mmm format.
  • YYYY = year
  • MM = month
  • DD = day
  • HH = hour (24 hour)
  • mm = minutes
  • SS = seconds
  • mmm = milliseconds
You can see a valid time or None if no event time is recorded.
Frequency Overrange Fault
Displays whether a frequency overrange fault is present on the counter.
Quadrature Error Count
Displays the number of times that a quadrature counter error occurred.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal