Device Definition – SSI view parameters
The
SSI
view in the Device Definition dialog includes these parameters:
Parameter | Description |
|---|---|
Enable Store via Input00 | Specifies whether the Store function is triggered using
Input00.
|
Invert Input00 | Specifies whether to invert the indicated input.
|
Provide Feedback