Device Definition – Output Assignments view parameters

The
Output Assignments
view in the Device Definition dialog includes these parameters:
Parameter
Description
Output
Displays the output number to which this configuration applies.
Selected Mode
Select the operation mode for the output or disable the output, if it is not in use.
  • Disabled
  • Controlled by Window
  • Pulse Width Modulation
  • Triggered Pulse
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal