Device Definition – Events view parameters
The
Events
view in the Device Definition dialog includes these parameters:
Parameter | Description |
|---|---|
Eventxx – User Defined Data x | Associates user-defined data instances with Events on the module.
You can choose as many as three instances for each event. When Encoder Type is configured as HSC:
When Encoder Type is configured as SSI:
|
Provide Feedback