Ptxx Diagnostics view parameters (5034-IB16, 5034-IB8)
The
Ptxx Diagnostics
view includes these parameters:
Parameter | Description |
|---|---|
Fault Exists | Displays whether a fault is present. |
Data Uncertain | Displays the module is operating outside the designed
operating range, or data is under manual or override
control. |
Field Power | Displays whether field power is present on the point. |
Field Power On Timestamp | Displays the timestamp of the last time field power turned on
in YYYY-MM-DD-HH:mm:SS.mmm format.
You can see a valid time or None if no event time was
recorded. |
Field Power Off Timestamp | Displays the timestamp of the last time field power turned
off in YYYY-MM-DD-HH:mm:SS.mmm format.
You can see a valid time or None if no event time was
recorded. |
Provide Feedback