Points view parameters (5034-OA4)

The
Points
view includes these parameters:
Parameter
Description
Enable DC mode
Determines whether DC mode is enabled. By default, the module operates in AC mode.
  • DC mode
    : The module operates in 10…250V DC.
  • AC mode
    : The module operates in 120/240V AC. The output switches ON or OFF only when the AC waveform crosses near 0V.
Point
Displays the point number to which this configuration applies.
Output State During Program Mode
Determines the behavior of each output when the controller transitions to Program Mode or Inhibit mode. While in Program Mode or Inhibit mode, outputs from the controller are ignored and the output behaves as follows:
  • Off – Output is 0 or Off.
  • On – Output is 1 or On.
  • Hold – Output maintains the last state.
Output State During Communication Fault Mode
Determines what happens to the output of each point after a communication fault occurs and the module enters Communication Fault Mode.
  • Off – Output is 0 or Off.
  • On – Output is 1 or On.
  • Hold – Output maintains the current level.
Communication Fault Mode Output State Duration
Determines the length of time the Communication Fault Mode is held before the Final Fault State.
Communication Fault Mode Output State Final State
Determines whether the module transitions to On or Off after the Communication Fault Mode Output State Duration elapses. The default final state is Off.
If you choose Forever for Duration, you cannot choose a final state. The module retains its current Communication Fault Mode state.
Mode When Communication Fails in Program Mode
Determines the output action if communication fails in Program Mode.
  • Program Mode – Indicates leaving outputs in Program Mode state.
  • Communication Fault Mode – Indicates changing outputs to Communication Fault Mode state.
Diagnostics
Opens the Diagnostics dialog, which contains diagnostic information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal