Points view parameters (5034-IB16, 5034-IB8)
The
Points
view includes these parameters:
Parameter | Description |
|---|---|
Point | Displays the point number to which this configuration
applies. |
Input Filter Time Off → On | Defines how long an Off to On input transition must remain in
the On state before the device considers the transition
valid. |
Input Filter Time On → Off | Defines how long an On to Off input transition must remain in
the Off state before the device considers the transition
valid. |
Diagnostics | Opens the Diagnostics dialog, which contains diagnostic
information. |
Provide Feedback