Points view parameters (5034-IA8)
The
Points
view includes these parameters:
Parameter | Description |
|---|---|
Point | Displays the point number to which this configuration
applies. |
Input Filter Time Off → On | Defines how long an Off to On input transition must remain in
the On state before the device considers the transition
valid. Valid values are:
NOTE:
For a module operating with a
120V AC input signal, the only valid Off to On filter
value is 1 ms.
|
Input Filter Time On → Off | Defines how long an On to Off input transition must remain in
the Off state before the device considers the transition
valid. Valid values are:
|
Provide Feedback