Domain name
Valid characters:
- Number range is 0…9
- Alpha characters in the range of A…Z (upper or lower case)
- dash
- period
- Maximum of 48 valid ASCII characters
- Do not use a period or a dash for the first and last character
- Use only alpha characters in the last portion
- Do not use two periods next to each other
Valid domain name format:
- a.b.c.d
- a.b.c
- a.b
- a
Legal domain names example:
- xyz.xxx.yyy.com
- 123.xxx.yyy.com
- 123.123.123.com
- 123.123.com
Illegal domain name example:
- 123.345.789.123
- 1234567890
- 123.
- .467
- 123..com
Provide Feedback