Loading
Press Release | May 18, 2017
Recent ActivityRecent Activity

Stratix 2500 Lightly Managed Switch Addresses Evolving Networking Needs

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
New industrial network switch from Rockwell Automation closes gap between unmanaged and managed switches

MILWAUKEE — Manufacturers that use unmanaged network switches but struggle with downtime or security concerns now have an alternative to using managed switches. The Allen-Bradley Stratix 2500 lightly managed switch from Rockwell Automation provides the security, resiliency, segmentation and bandwidth-optimization benefits of a managed switch without the need for extensive configuration. 

“Unmanaged switches deliver the network connectivity required for less complex industrial applications, but they can’t provide diagnostics, manage traffic or enhance security,” said Divya Venkataraman, global product manager, Rockwell Automation. “Manufacturers need a more robust switch when issues like packet storms are bringing down their network, or if they want to protect against growing security threats. This is where a lightly managed option like the Stratix 2500 switch delivers exceptional value.”

When installed straight out of the box, the Stratix 2500 industrial Ethernet switch can prioritize critical industrial network traffic. It also can be configured for application-specific needs. Manufacturers can use this flexibility to futureproof their operations by deploying the switch out of the box today and scaling it up to a lightly managed switch as their needs evolve. 

As a lightly managed switch, the Stratix 2500 switch far exceeds the capabilities of an unmanaged switch by monitoring and optimizing traffic flow and providing diagnostic information to help minimize downtime. It also can support up to 64 VLANs for logical segmentation, which helps reduce total cost of ownership. In addition, port security allows users to disable ports or control end-device connectivity based on the media access control address.

The Stratix 2500 lightly managed switch uses embedded Cisco technology and is part of the Rockwell Automation Integrated Architecture system. This helps ease network configuration, management and support while optimizing integration with the enterprise network. 

“With embedded Cisco technology, the Stratix 2500 switch delivers the security and monitoring capabilities required by IT professionals while exposing an easy-to-use web interface for operations professionals,” said Samuel Pasquier, director of product management, IoT Platforms, Cisco. 

The switch is another result of the ongoing collaboration between Rockwell Automation and Cisco to provide industrial networking solutions that help manufacturers on their digital transformation journey.

News Release Asset
Image available upon request or here at box.com.

About Rockwell Automation 
Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs approximately 22,000 people serving customers in more than 80 countries. 

Media Contacts 
Tiffany Pfremmer
Rockwell Automation
414.382.4814
tbockhop@ra.rockwell.com 

Leanne Hanson
Padilla
612.455.1776
leanne.hanson@padillaco.com 

Allen-Bradley, Integrated Architecture and Stratix are trademarks of Rockwell Automation Inc.

Published May 18, 2017


  1. Chevron LeftChevron Left Rockwell Automation Home
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Press Releases
  5. Chevron LeftChevron Left Stratix 2500 Lightly Managed Switch Addresses Evolving Networking Needs