You may also be interested in
CAM Technologies provides expert system analysis, solutions design and implementation, and remote monitoring capabilities for compressed air technologies.
DENSO is a global company focused on advanced mobility that positively changes how the world moves and contributes to greater well-being. As a global Fortune 500 company, DENSO has a broad product portfolio and widespread global impact.
- Meet corporate decarbonization goals
- Reduce scope 2 emissions
- Integrate 3 air compressors and 2 air dryers into the compressed air system
- Provide advanced PLC-based automation to optimize equipment operation across a varied demand profile
- Track efficiency data and leverage analytics to maintain efficiency long-term
- Circuit & Load protection: Circuit breakers, fuse holders
- Connection Devices: Network media, terminal blocks
- Energy Monitoring: PowerMonitor1000
- HMI: Panelview Plus 7 Performance HMIs
- Networking: Stratix® series switches
- Programmable Controllers: CompactLogix 5380 Series PLCs and I/O
- Push Buttons & Signaling Devices: 22mm Operators, audio/visual devices
- Relays & Timers: General-purpose relays
- Sensors & Switches: Condition sensing – pressure sensors
- FactoryTalk® View
- Studio 5000®
- FactoryTalk® Linx
- Integrated Architecture® Builder
- 26% reduction in energy used for compressed air
- 3,110 metric tons/year in carbon reduction
- $350,000 energy cost savings per year realized
CAM Technologies, a Rockwell Automation PartnerNetwork™ Program participant, has been exclusively using Rockwell components for over 30 years across their entire product portfolio. For this project, CAM Technologies was brought in by DENSO, a leading tier 1 auto supplier, to help them reduce scope 2 emissions. In addition to advancing DENSO’s net zero goals, the project modernized the compressed air system through the installation of three new compressors, two new dryers, and the complete elimination of R-22 refrigerant previously used in six non-cycling air dryers.
DENSO’s existing relationship with CAM Technologies was a key factor in selecting them to lead efforts to enhance operational efficiency and reduce the environmental impact of the compressed air system at their thermal manufacturing facility in Battle Creek, Michigan.
On this particular project, CAM Technologies partnered with Energy Systems Group (ESG) to conduct a comprehensive, site-wide energy study. “The study gave us baseline metering data and helped to identify system opportunities relating to power consumption, air pressure, air demand, compressed air flow. Using the data, we created a turnkey solution for DENSO,” Jeff Kahn, of CAM Technologies said.
The results from the analysis formed the basis of the design and installation of a state-of-the-art system featuring high-efficiency compressors and air dryers, optimized piping, and the CAMLink Premier Compressed Air Automation System powered by an Allen Bradley CompactLogix® controller.
Challenge
DENSO’s corporate office set an ambitious goal to be carbon neutral in all facilities by 2035. To achieve this goal, DENSO’s manufacturing facility in Battle Creek, Michigan engaged Energy Systems Group (ESG), a consumer energy organization, to perform a full factory energy audit. ESG determined that a critical next step toward compliance with the corporate scope 2 emission reduction goal was to optimize energy use on the factory’s air compressors. At this facility, part of DENSO’s North American Thermal (TAC) business, they manufacture automotive air conditioning and engine cooling components and systems.
Compressed air is a common power source in factories, but it’s also notoriously inefficient – with as much as 80% of the energy going into compressors being lost as waste heat. The Battle Creek’s factory’s compressors were running constantly – overnight, on weekends and holidays, and regardless of how loads changed during manufacturing. As an additional challenge, some of the older compressors were installed when the facility was first built 30 years ago, making those even less efficient than newer models. Most compressors operated continuously, regardless of actual demand, and the facility lacked a centralized control system to coordinate compressor usage for optimal efficiency.
Solution
DENSO’s Battle Creek facility decided to engage CAM Technologies, a gold-level member of the Rockwell Automation PartnerNetwork™ program, to develop a solution to automate and modernize their compressed air system. CAM Technologies managed the full scope of the project from equipment procurement to final commissioning.
CAM Technologies relies on Rockwell Automation for its industrial automation solutions. They have a mature software product designed to optimize the operation of any multi-compressor compressed air system regardless of brand or technology. Their solution can be easily designed, configured, and deployed – which maximizes return on investment.
To modernize DENSO’s compressed air systems, CAM Technologies delivered a solution that used Allen-Bradley® circuit and load protection, circuit breakers, fuse holders, network media, switches, signaling devices, relays and terminal blocks. PanelView™ Plus 7 Performance HMIs were used to give operators visibility and ability to control the system. PowerMonitor1000 was used for energy monitoring and optimization. And control for the system was built using CompactLogix 5380 Series PLCs.
Having the new system connected to the building automation means DENSO now has full control over when a compressor runs and when it can sit idle without drawing much power. Having this level of control means energy use is down and so are emissions.
Result
By updating the compressed air systems, replacing three of the oldest ones, and connecting them all to the facility’s building automation system, it’s now possible to cycle the compressors in sync with demand, instead of running continuously. DENSO has seen a significant cost savings along with a reduction in energy use.
Data is collected, stored in the cloud, and displayed on dashboards. This data can be used to maintain efficiency long term, while also making it easier to identify operational problems quickly.
DENSO has seen a measured carbon reduction because of this project: 3,110 metric tons/year. To put that into context, it is the equivalent of electricity used in more than 700 homes annually.
“DENSO now has real-time and historical visibility into all major energy and cost components of the compressed air system, which includes pressure, mass flow, dew point, and power. Access to data and analytics can be used to show patterns of energy waste that can build between audits and go unseen during a walk through,”
Published April 7, 2026