Access the FactoryTalk Linx RMCT

Once you have installed the
FactoryTalk® Linx
Redundancy Module Configuration Tool (RMCT), you can launch the tool from the
FactoryTalk® Linx
network browser.
If you use
FactoryTalk® Security
, you must have Open Device Configuration permission to access the tool. To configure Open Device Configuration permission, open
FactoryTalk® Administration Console
, and then go to System > Policies > Product Policies > FactoryTalk Linx > Feature Security.
Open Device Configuration Setting
Open Device Configuration setting in FactoryTalk Security
To access the
FactoryTalk® Linx
RMCT in the
FactoryTalk® Linx
network browser, the Enable Device Configuration setting must be selected. To verify that this setting is selected, open the
FactoryTalk® Linx
network browser, and then open Advanced Settings.
Enable Device Configuration Setting
Enable Device Configuration setting in the FactoryTalk Linx network browser
To access the
FactoryTalk® Linx
RMCT, follow these steps.
  1. Launch the
    FactoryTalk® Linx
    network browser.
  2. Browse to your redundancy module.
  3. Right-click the redundancy module and select Device Configuration.
    IMPORTANT: If you cannot see the Device Configuration menu option, then the compatible version of the
    FactoryTalk® Linx
    RMCT is not installed. For more information, see Identify the RMCT Version.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal