Logix SIS Considerations

Read and understand the following safety concepts that apply to Logix SIS:
  • SIL 2 and SIL 3 requirements
  • Safety task requirements
  • Safety task execution
  • Safety function muting
  • Safety signature validation
  • Recommended safety I/O settings
  • Safety data
To configure a redundant controller for Logix SIS, see Configure Logix SIS Requirements.
For general information about safety application development, including the safety signature, commissioning lifecycle, reaction times, and safety application instructions, see the ControlLogix 5590 Controllers User Manual, publication 1756-UM900.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal