Outputs View

Use Outputs to view or configure the outputs for the device.
Outputs View Example
The Outputs view includes these parameters:
Parameter
Description
Output
Displays the output number to which this configuration applies.
Mode
Displays the mode for the output.
Output State in Program Mode
Determines the behavior of each output when the controller transitions to Program Mode or Inhibit mode. While in Program Mode or Inhibit mode, outputs from the controller are ignored and the output behaves as follows:
  • Off – Output is 0 or Off.
  • On – Output is 1 or On.
  • Hold – Output maintains the last state.
  • Local Control – Output continues to be controlled by the window.
Output State in Communication Fault Mode
Determines what happens to the output of each point after a communication fault occurs and the module enters Communication Fault Mode.
  • Off – Output is 0 or Off.
  • On – Output is 1 or On.
  • Hold – Output maintains the last state.
  • Local Control – Output continues to be controlled by the window.
Diagnostics
Opens the Diagnostics dialog, which contains diagnostic information.

Outputxx Diagnostics

To view the Outputxx diagnostics, select Diagnostics Outputs view.
Outputxx Diagnostics Example
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal