Rolling Timestamp of Dynamic/Device Variable Data

Whenever a HART module receives new HART Dynamic or Device variable data from a HART device, the module also records the value of RollingTimestamp at that time. The Logix 5000 controller uses the last two rolling timestamp values to calculate the amount of time between the samples.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal