Producer/Consumer Data Configuration

The Producer/Consumer data can be configured to include the following for each HART device:
  • Up to four dynamic variables
  • Up to eight device variables
  • Up to four HART commands
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal