Producer/Consumer Communication of HART Device
The Producer/Consumer communication between controller and HART device allows you to:
- Monitor HART device status or configuration change.
- Get PlantPAx specific data required for the PlantPAx HART instruction.
- Get periodical update of dynamic variable data and status.
- Get periodical update of device variable data and status.
- Execute HART commands on-demand.
Provide Feedback