Channel Offset

The Channel Offset feature compensates for any known error on the actuator or channel to which the actuator is connected. The value is set in the Engineering Units and is added to the output data.
For example, consider an application that uses the Current (mA) input type with the 4…20 mA range and scaling at 0…100%. If a channel used in the output range 4…20 mA has an error that results in it consistently outputing 7.8 mA when O.Chxx.Data is 8 mA, you must account for the error by setting the Channel Offset to 1.25.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal