Connection View
Use this view to complete the following tasks:
- Set the RPI rate. All HART devices attached to the same HART module share the same RPI rate.
- Set the connection type to use on the EtherNet/IP network.
- Inhibit the device.
- Configure fault response for connection failure while the controller is in Run mode.
TIP:
The Module Fault area of the Connection view is
useful for troubleshooting.
WARNING:
You cannot test the process data output of an
output device while the device is inhibited.

Provide Feedback