Preface
About This Publication
This manual describes how to use the PointMax high-speed counter/serial synchronous
interface (SSI) encoder module in Logix 5000® control systems.
Make sure that you are familiar with the following:
- Use of a controller in a Logix 5000 control system
- Use of an EtherNet/IP™ network
- Studio 5000 Logix Designer® environment
Provide Feedback