Encoder Module Applications

This chapter describes how to configure your high-speed counter/SSI encoder module in aStudio 5000 Logix Designer application project. You can use the default module configuration oredit the module configuration.
This chapter does not explain the user-configurable module features that you can edit on different screens in your Studio 5000 Logix Designer application project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal