Override Inputs

You can override the state of module inputs. This practice is commonly used when troubleshooting an application or testing a control system outside normal operating conditions.
You must change the following tags to override the input state:
  • O.Counterxx.OverrideDataxEn – Set the tag to 1 to enable the O.Counterxx.OverrideDataxValue to override the input state.
  • O.Counterxx.OverrideDataxValue – Set the tag to the desired value.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal