Search
PointMax High-speed Counter/SSI Encoder Module
Counter Modes
This section describes the types of counter modes that are available when the module is configured in HSC mode.
High-speed Counter (HSC) Input
Count/External Direction Mode
Count/Internal Direction Mode
Up and Down Pulses Mode
X1 Quadrature Encoder Mode
X2 Quadrature Encoder Mode
X4 Quadrature Encoder Mode
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal