Configure Counter State When Module is in Program Mode or Inhibited
You can configure the counter to specific states when the module is in Program Mode or
when the module is inhibited.
When the controller switches from Run mode to Program Mode or Inhibited, the counter can
behave in the following ways, depending on how you configure the Counter State in
Program Mode parameter:
- Continue counting – Default
- Hold its last state
- Transition to a user-defined value
You can choose to reset the stored values when the module is in Program Mode or
Inhibited.
When the module is inhibited, the counter behavior follows the Counter State in Program
Mode configuration.
Provide Feedback