Standard Module Applications
This chapter describes how to configure your serial module in a Studio 5000 Logix
Designer application project. You can use the default module configuration or edit the
module configuration.
This chapter does not explain the user-configurable module features that you can edit on
different screens in your Studio 5000 Logix Designer application project.
Provide Feedback