Master Command List Function Codes

Master command list function codes are:
  • Read Coil Status (Function Code 01)
  • Read Input Status (Function Code 02)
  • Read Holding Registers (Function Code 03)
  • Read Input Registers (Function Code 04)
  • Force Single Coil (Function Code 05)
  • Preset Single Register (Function Code 06)
  • Force Multiple Coils (Function Code 15)
  • Preset Multiple Registers (Function Code 16)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal