Add a New Module to a Studio 5000 Logix Designer Application Project
You must complete the following tasks before you configure the module:
- Create a Studio 5000 Logix Designer application project.
- Add a Logix 5000 controller to the project.
- Add a PointMax EtherNet/IP adapter to the project.For more information on how to add a PointMax EtherNet/IP adapter to the Studio 5000 Logix Designer application project, see the PointMax EtherNet/IP Adapter User Manual, publication 5034-UM001.
After completing above steps, add your I/O module to the project by following one
of the methods:
- Discover Modules
- New Module
Provide Feedback