Module Firmware Updates

I/O modules are manufactured with module firmware installed. If updated module firmware revisions are available in the future, you can update the firmware.
Firmware information for I/O modules is available at the Rockwell Automation Product Compatibility and Download Center (PCDC). The PCDC is available at: rok.auto/pcdc. At the PCDC, you can use the module catalog number to check for firmware updates. If the catalog number is not available, then no updates exist.
IMPORTANT:
Only download firmware and access product release notes from the Rockwell Automation PCDC. Do not download firmware from non-Rockwell Automation sites.
Verify that the firmware revision of the I/O modules that you use is correct before commissioning the system. For more information on how to update your module firmware, see the ControlFLASH Plus® Quick Start Guide, publication CFP-QS001.
When the firmware update is in progress, you cannot perform the following operations:
  • Another firmware update request
  • Module connection request
  • Module reset request
WARNING:
When you update the PointMax EtherNet/IP adapter firmware, the I/O modules in its chassis may reset and unable to maintain their Program Mode or Inhibit Mode states. Verify that all equipment controlled by the modules in this chassis is in a stopped state and that all safety-critical functions are unaffected.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal