Protected Operations
If one of the module I/O connections is open and running, it is considered as the module
is in Protection Mode. Protection Mode is a state where the device is operational but
has implemented defenses against disruptive changes that could take the product out of
service. The following operations are restricted when the module is in Protection
Mode:
- Firmware update request
- Module reset request
- Module calibration request
- Connection or data format change
The following operations can be applied in Studio 5000 Logix Designer application when
the module is in Protection Mode but as a consequence, the I/O connections are closed
and reopened:
- Change Electronic Keying
- Change RPI
- Change Unicast/Multicast
The following operations are allowed when the module is in Protection Mode:
- Listen-only connection requests from other controllers
- I/O channel configuration change. To apply configuration change without interrupting the I/O connections, there are two methods:
- Change configurations and apply in Module Properties.
- Change configuration tag values and send a Reconfigure Module MSG to the module to apply the changes
TIP:
Inhibit the module to come out of the Protection Mode.
Provide Feedback