Open Wire Detection
Open Wire detection detects when a wire is disconnected from the channel. For
5034-IF4/IF8C/IF8V module, to enable Open Wire detection, go to Channels → Chxx view in
Module Properties and select Enable Open Wire Detection checkbox. For 5034-IRT4I module,
Open Wire detection is always enabled.
For 5034-IRT4I module, the value that is reported during an Open Wire detection depends
on the Diagnostics selection (minimum/maximum engineering) on the channel. See Chxx View to set the diagnostic condition.
Mode | Cause of Detection | Resulting Module Behavior |
|---|---|---|
Current (mA) | The input signal for a channel is below 92 μA. |
|
Voltage (V) | The input signal value is above 11V. |
|
Mode | Cause of Detection | Resulting Module Behavior |
|---|---|---|
RTD | A wire is disconnected from the channel. |
|
Thermocouple |
IMPORTANT:
The Disable All Alarms feature does not disable the Open Wire detection feature but
it disables all alarms on the module.
The Open Wire detection feature is not an alarm. It is an indicator that a wire has
been disconnected from the channel but does not trigger an alarm.
For 5034-IF4, 5034-IF8C, and 5034-IF8V modules, to disable the Open Wire detection
feature, you must clear the Enable Open Wire Detection checkbox in the Chxx
view.
For 5034-IRT4I module, open wire detection is always enabled. You can disable the
channel if it is not in use.
Provide Feedback