Rolling Timestamp of Data
Rolling timestamp represents the time when the current
I.Chxx.Data
is sampled. It
is a continuously running 15-bit rolling timestamp that counts in milliseconds from
0…32,767 ms. The rolling timestamp value is reported in the
I.Chxx.RollingTimestamp
tag for the analog I/O modules.The controller program uses the last two rolling timestamp values to calculate the amount
of time between the samples.
A system time change can cause a slight change in input sample timing. The rolling
timestamp accurately reflects the change. There can be jitter in the timing between
samples before and after the system time change.
Provide Feedback