Per Point Input Timestamping
As a Sequence of Events feature, you can configure an input point to timestamp the input
transitions and report the timestamps on per-point basis. The timestamps are based on
the system time clock from CIP Sync.
Pulse Latching
Pulse Latching is supported via the Timestamping feature and Timestamp Latching. You
can use Pulse Latching to detect or latch short-duration pulses.
To use Pulse Latching, you must set the Input Data parameter to Timestamp Data in the
Device Definition dialog.
Location in Studio 5000 Logix Designer Application
Project | Action |
|---|---|
Module Properties → Points → Ptxx | Check the input transition type where you must latch
short-duration pulses. For example, for short-duration pulses that are latched for
Off to On transitions, select Off → On input transition. |
Module tags | One or both of these actions.
|
When the module detects a short-duration pulse at an input point, the changes that
are described in this table occur.
Input Transition Type Where Pulse Is Captured | Change in Studio 5000 Logix Designer Application Project |
|---|---|
Off to On |
|
On to Off |
|
When subsequent short-duration pulses are detected at the same input point, the
Latching configuration dictates what changes, if any, occur in the Studio 5000 Logix
Designer application project.
Latching Configuration | Input Transition Type Where Pulse Is Captured | Change in Studio 5000 Logix Designer Application Project |
|---|---|---|
Disabled (default) These conditions disable Timestamp Latching.
| Off to On | The I.Ptxx.TimestampOffOnNumber tag increments.The new time stamp is recorded in the
I.Ptxx.TimestampOffOn tag, which overwrites the
previous time stamp. |
On to Off | The I.Ptxx.TimestampOnOffNumber tag increments.The new time stamp is recorded in the
I.Ptxx.TimestampOnOff tag, which overwrites the
previous time stamp. | |
Enabled These conditions enable Timestamp Latching.
| Off to On | The I.Ptxx.TimestampOffOnNumber and
I.Ptxx.TimestampOffOn tags remain latched until the
last captured pulse is acknowledged. In other words, the tag
values remain the same until the last captured pulse is
acknowledged. |
On to Off | The I.Ptxx.TimestampOnOffNumber and
I.Ptxx.TimestampOnOff tags remain latched until the
last captured pulse is acknowledged. In other words, the tag
values remain the same until the last captured pulse is
acknowledged. |
To acknowledge the last captured pulse, set the output tag of the last input pulse as
follows:
- Off to On transition - Set theO.Ptxx.TimestampOffOnNumberAcktag =I.Ptxx.TimestampOffOnNumbertag.
- On to Off transition - Set theO.Ptxx.TimestampOnOffNumberAcktag =I.Ptxx.TimestampOnOffNumbertag.
Once a pulse latch is acknowledged for an input point, the next pulse at that point
increments the corresponding
I.Ptxx.TimestampOffOnNumber
and records the time
stamp in I.Ptxx.TimestampOffOn
.You can change tag values in program logic while normal module operation continues or
through the Studio 5000 Logix Designer application tag editor.
Chatter Detection
Chatter Detection is a feature that is directly related to Timestamping. You use the
feature to detect when a device that is connected to the module input causes
chatter.
Chatter occurs when the device causes the inputs to transition falsely many times in
a relatively short period. As a result, the module time stamps invalid input
transitions.
You can configure the following:
- Chatter Count – Determines the number of acceptable input transitions that can occur in a given time period before considering the input to be chatter.
- Chatter Time – Determines the amount of time within which the number of input transitions are counted.
Provide Feedback