Field Power (SA Power) Loss Detection
The Field Power Loss Detection feature monitors for the loss of field-side power on the
SA power bus.
The Field Power Loss condition causes safety connections to fault. The module does not
send anything to the controller until the controller queries the diagnostic
assembly.
In the diagnostic assembly, the FieldPowerOff bit is set at the module and point level
structure. The Fault bit is set at the point level.
Provide Feedback