Connection Fault Handling

You cannot configure the safety output module behavior when a connection fault occurs, that is, the connection between the owner-controller and the output module breaks. All outputs are put in a Safe state.
The output remains in a Safe state until the connection to the owner-controller is re-established. The output returns to normal operation as defined in the module configuration.
Once the connection between the owner-controller and output module is re-established, the output resumes normal operation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal