Safety Output Modules in CIP Safety Systems

The following apply to the safety outputs:
  • You can connect safety devices, such as safety relays, safety contactors.
  • An external wiring short-circuit check between channels or supply is possible when the safety output is configured as Safety Pulse Test mode. The detection of external wiring fault is ≤ 1024 msec.
  • Diagnostics. See Status and Fault Information in Module Properties.
  • Safety output points are configured as the following:
    • Not Used
    • Safety
    • Safety Pulse Test

Safety Mode and Safety Pulse Test Mode

The Safety Output can be configured to two types of point modes:
  • Safety Mode
  • Safety Pulse Test Mode
Safety Mode
When the safety output is configured to Safety Mode, a warning message prompt occurs.
You are responsible to command the Safety Output to Safe State at the stated interval in order to achieve the desired safety level.
Safety Pulse Test Mode
When the safety output is configured to Safety Pulse Test Mode, the safety output channel continuously test the ability of the safety output to remove power from the output terminals of the module. The safety output turn off momentarily during the pulse test duration.
If an error is detected, the safety output data and individual safety output status turn off.
Safety Output Voltage Variation During Pulse Test When Safety Pulse Test Mode is Configured
On the safety output modules, the pulse width (X) is less than 700 μs, and the pulse period (Y) is less than 524 ms.
TIP:
To help prevent the test pulse from causing the connected device to malfunction, pay careful attention to the input response time of the output device.
See Wiring Diagrams for Safety Mode and Safety Pulse Mode for more details about applying Safety Mode and Safety Pulse Test Mode in your application.

Single-channel Mode

When the output channel is in the On state and without any faults, the safety outputs turned on. The status is normal. If a fault is detected on the output channel, the safety output is de-energized and individual safety output status turn off.
Single-channel Normal Operation and Fault Detection (Not to Scale)

Dual-channel Mode

When dual-channel mode is used, output channels function as connection pairs. Connection pairs are as follows:
  • Channels 0 and 1
  • Channels 2 and 3
  • Channels 4 and 5
  • Channels 6 and 7
When both output channels in a connection pair are in the On state and without any faults, the safety outputs are turned on.
Dual-channel Normal Operation and Fault Detection (Not to Scale)

Surge Capability of Safety Output

The safety output supports temporary surge of current when transitioning from OFF to ON.
Surge Capability

Safety Output Fault Reset

The I/O channel supports a module-level user-configurable ‘Latch Fault until reset via output tag’ mode and recovers from only these field faults:
  • Safety Output Overload
  • Safety Output NoLoad
TIP:
Other types of Safety Output faults are non-recoverable. You must cycle power to the module.
Latch Fault until Reset via Output Tag mode is Enabled
When Latch Fault mode is Enabled, the I/O channel holds safety output fault indications until it checks that the field fault is removed. If the field fault is removed, the channel clears the fault status only upon detecting that the ResetFault in its consume assembly channel sees a rising edge.
Latch Fault until Reset via Output Tag mode is Disabled
When Latch Fault mode is Disabled (default), the I/O channel holds safety output fault indications for 1 second until it checks if the field fault is removed. If the field fault is removed, the channel clears the fault status only upon detecting the consume data bit is low. The fault status can also be cleared by a module reset or power cycle.
After the channel clears the fault, the I/O indicator (red) turns off. The output data can now be controlled.
IMPORTANT:
If the module outputs experience persistent high faults, consider cycling power to the module to clear the error.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal