Connection Optimization
PointMax I/O system supports automatic optimization for I/O connections.
The following conditions must be met for connections to be included in the
optimization:
- I/O modules on the rack have the same RPI
- Unicast
- Sum of data sizes are within the packet limit
This is similar to how I/O systems such as POINT I/O™ support rack
optimization or enhanced rack optimization. Functional safety modules, HART modules, and
IO-Link master modules are excluded from the optimization.
Provide Feedback