Preface

About This Publication

This manual describes how to use PointMax™ EtherNet/IP™ adapters in Logix 5000® control systems. Use this manual in conjunction with the EtherNet/IP Network Devices User Manual, publication ENET-UM006.
Make sure that you are familiar with the following:
  • Use of a controller in a Logix 5000 control system
  • Use of an EtherNet/IP network
  • Studio 5000 Logix Designer® application environment
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal