Set the Network Address with the Rotary Switches

If the network uses 192.168.1.x, use the rotary switches on the adapter to set the last octet of the network IP address. Valid numbers range from 001…254.
IMPORTANT:
The rotary switches only set the IP address when power is cycled.
WARNING:
When you change switch settings on the adapter while power is on, an electric arc can occur. This could cause an explosion in hazardous location installations. Be sure that power is removed or the area is nonhazardous before proceeding.
If you change the rotary switches when the device is powered up, a minor recoverable fault occurs on the device in order to alert you of an unexpected configuration change. The change will only take effect after cycling power or after a reset.
Rotary switches – The bottom switch represents the first digit in the octet, the middle switch represents the second digit, and the top switch represents the third digit.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal