Set the Network Address with FactoryTalk Linx Software
- Use the FactoryTalk Linx Network Browser to navigate to the device and select the wrench icon.

- Enter the IP address settings.

Provide Feedback