To select one of the network redundancy modes, do the following:
- Power down the adapter.
- Use the PRP/DLR rotary switch to select the redundancy mode.
- The black x100 rotary switch positions on the left set the adapter to PRP mode.
- The white x100 rotary switch positions on the right set the adapter to DLR mode.
- Power up the adapter.
Before you select one of the redundancy modes, verify your network settings to determine
the redundancy mode used by your network.
IMPORTANT:
The rotary switches only set the IP address
when power is cycled.
IMPORTANT:
If you switch the adapter to a redundancy mode that is different from your network, the
adapter disconnects from the network.
IMPORTANT:
You cannot switch the network redundancy mode while the adapter is running. A minor
recoverable fault occurs to warn about the unintentional change to the network redundancy
mode.
Provide Feedback