PointMax Adapter Status Indicators

EtherNet/IP communication modules have bicolor status indicators to assist with performance and diagnostics.
PointMax EtherNet/IP Adapter Status Indicators
A - Module Status Indicator
Indicator
State
Description
MOD
Off
The adapter is not powered.
Steady green
The adapter is operational.
Steady red
The adapter is in power-up state or in an unrecoverable fault state.
Flashing red/green
The adapter is in self-test mode.
Flashing red
The adapter is in one of the following states:
  • Factory default power-up
  • Recoverable fault
  • Firmware update in progress
Flashing green
The adapter is in standby mode.
B - Network Status Indicator
Indicator
State
Description
NET
Off
The network is in one of the following states:
  • The adapter is not powered
  • The adapter is powered but there is no IP address configured
Steady green
A network connection is established and at least one CIP™ connection is established.
Steady red
A duplicate network address is detected.
Flashing red/green
The adapter is performing power on self test (POST).
Flashing red
The network connection has timed out.
Flashing green
A network address is configured but there are no CIP connection established.
C - LINK 1 Network Status Indicator
Indicator
State
Description
LINK 1
Off
No Ethernet cable is connected.
Flashing green
Communication is active through the connected Ethernet cable.
Flashing red
The adapter is operating in PRP mode and a LAN A warning has occurred.
D - LINK 2 Network Status Indicator
Indicator
State
Description
LINK 2
Off
The network is in one of the following states:
  • No Ethernet cable is connected
  • The adapter is the active ring supervisor in a DLR network and has detected a rapid ring fault.
Flashing green
Communication is active through the connected Ethernet cable.
Steady green
The adapter is the active ring supervisor in a DLR network and the ring is not broken.
Flashing red
The adapter is operating in PRP mode and a LAN B warning has occurred.
E - Module Power Status Indicator
Indicator
State
Description
MOD PWR
Off
Module power is not available.
Steady green
Module power is available.
F - SA Power Status Indicator
Indicator
State
Description
SA PWR
Off
SA power is not available.
Steady green
SA power is available.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal