Marine Application Considerations
When you install a PointMax I/O system in a marine application, consider the following
exceptions:
- A Salt Test is not performed on the PointMax I/O system because you must install the system in an IP54 rated enclosure. The enclosure that is used in the final installation might require a Salt Test if it is installed in the exposed area.
- A Compass Safe Distance test is not performed on the PointMax I/O system. If the system is installed on the navigation bridge of a marine vessel, it must be placed outside the 5 m (16.4 ft) radius from the compass.
- An Acoustic Noise test is not performed on the PointMax I/O system because it does not produce noise or alarms that can interfere with marine vessel safety signals.
For more information, see the certificate details available on the Product Certification
website at rok.auto/certifications.
Provide Feedback