Rack Orientation

The PointMax I/O system can be oriented in the following positions:
IMPORTANT:
The maximum ambient temperature range differs by orientation.
  • -25 °C ≤ Ta ≤ +60 °C (-13 °F ≤ Ta ≤ +140 °F) for horizontal orientation
  • -25 °C ≤ Ta ≤ +55 °C (-13 °F ≤ Ta ≤ +131 °F) for other orientations
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal