Remove the I/O Module

  1. After removing the RTB, hold the I/O module with your index finger and thumb and press down on the lever at the top of the I/O module.
    hold the I/O module and press down on the lever
  2. Unlock the I/O module.
  3. Pull the I/O module straight out of the mounting base.
    pull the I/O module out
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal