Install the RTB
Before you can install the RTB on the I/O module, you need to insert the RTB key into the
key slot for it to be compatible with the I/O module that you choose to install the RTB
on.
- Hook the RTB pivot clip to the I/O module’s mounting base.
- Pivot the RTB handle until it locks onto the I/O module.
- Repeat the above steps for all other I/O modules (if necessary). Make sure to lock the RTB handle after installation.
Provide Feedback