Install the Shield Clamps or Wire Holders (optional)

You can install a shield clamp or wire holder into the RTB slot to secure the cables with cable ties.
Shield clamp is a 1-wire shield clamp (5034-SHIELD) - Use it to clamp a shielded cable with outer jacket diameter of 5.5...8.0 mm (0.22...0.31 in.).
To install a wire holder or a shield clamp, proceed as follows:
  1. Insert a wire holder or a shield clamp into the RTB slot in the correct orientation as shown.
  2. If you installed a wire holder, place the cables on the wire holder and secure the cables with a cable tie.
  3. If you installed a shield clamp, secure the shielded cable on to the shield clamp with a cable tie.
  4. Install a 2.8 x 0.5 mm (0.11 x 0.02 in.) slip on connector to the grounding plate.
    Item Number
    Description
    A
    RTB
    B
    Wire holder
    C
    1-wire shield clamp
    D
    Cables
    E
    Single shielded cable
    F
    Cable tie
    G
    Slip on connector 2.8 x 0.5 mm (0.11 x 0.02 in.)
Recommended Wire Dressing
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal